Rexnord Introduces KleanTop Plastic Modular Belts for Food Processors

placeholder
Milwaukee, WI (USA) – Rexnord is proud to announce its new KleanTopTM plastic modular belting product line, specifically designed for the unique needs of the food processing industry.

“Food processors have requirements specific to hygiene and sanitation that few industries face.” said Lucas Knapp, Global Director of Marketing for the food industry. “With the KleanTop product line, food processing end users and OEMs can be sure the plastic modular belting they install is comprised of food-safe materials, meets the wash-down and abrasion resistant requirements for their applications, and are not a one-size-fits-all solution that may compromise quality or efficient operations.”

The KleanTop line launches with the introduction of new belting series designed specifically for the food processing industry: the Rexnord 590, 1090 and 1010 Series KleanTop belts. They join several other Rexnord belting products under the KleanTop line that feature food safe materials and designs, most notably the 390, 2010 and 1200 series. Each KleanTop product offers a set of benefits specific to the food processing industry, such as open hinges for cleaning and drainage, abrasion resistance and features that reduce product contamination concerns.

About the New Rexnord 590, 1090 and 1010 Series KleanTop Plastic Modular Belts:
  • The Rexnord 590 Series KleanTop is a ½” pitch belt designed to deliver an optimal combination of ease in cleaning, transfer capability and open area.
  • The Rexnord 1090 Series KleanTop offers the same benefits as the 590 Series. It is available in a 1” pitch and is optimized for use with a 2” diameter roller for smooth transfer and to promote airflow across the bottom of the belt.
  • The Rexnord 1010 Series KleanTop features an open hinge design with 60% rod exposure allowing for effective cleaning.
Rexnord manufactures both the KleanTop line of plastic modular and metal conveyor belting products, giving food processors a complete end-to-end solution for conveying systems.
 
Visit Rexnord.com/KleanTop for more information about the hygienic, food safe products within the new KleanTop line.
 
Visit Rexnord.com/590KleanTop for more information about the 590 Series KleanTop.
Visit Rexnord.com/1090KleanTop for more information about the 1090 Series KleanTop.
Visit Rexnord.com/1010KleanTop for more information about the 1010 Series KleanTop.
 
About Rexnord
Within Rexnord, we design, manufacture, market and service specified, highly engineered mechanical components worldwide used within complex systems where our customers’ reliability requirements and the cost of failure or downtime are extremely high. We keep industry moving with products and services that enhance the reliability of equipment supporting key industries, including food, beverage & liquid, automotive, energy, and mining. Rexnord acquired Cambridge Engineered Solutions in 2016 and is now the world’s largest manufacturer of metal and plastic conveyor chains and belts. Our new digital productivity platform, DiRXN (pronounced “Direction”), based on the integration of innovative Industrial Internet of Things (IIoT) and e-commerce technologies with a leading portfolio of tools, products and services, connects our customers to data and information that allows them to optimize productivity across all stages of their lifecycles.