Blog

Filters Reset
Sign up to get the latest updates from Rexnord!
Blog Thumbnail
Author: Marlon Casey | Category: Bearings
For industrial fan and blower applications, heavy-duty ball bearings, like the Rexnord Link-Belt Series 300, deliver high capacity, high speed and minimal vibration with less maintenance and turnover than roller bearings. Let’s look at the key advantages, as well as head-to-head test results.
Blog Thumbnail
Author: Mike Martin | Category: Bearings
Rexnord bearings are found in a wide range of applications under the fan and blower umbrella, from applications such as beverage air conveyors, cooling towers and cement dust removal fans, among others.
Blog Thumbnail
Author: Mark Czubak | Category: Bearings
On commercial fans and blowers, a large portion of the spherical roller bearings are mounted pillow blocks. Pillow blocks are convenient and offer an array of options to suit most applications. In general, pillow blocks come in two types: split housed solid housed.
Blog Thumbnail
Author: Jason Ludwig | Category: Bearings
In the fan and blower industry, selecting the right bearing for your application is crucial for bearing uptime and performance. This is where Rexnord's General Bearing Analysis Application can help. This tool was developed to select bearings that best match your application and analyze selected bearings to verify compatibility.
Blog Thumbnail
Author: Dale Stallard | Category: Bearings
Industrial fans and blowers commonly use both a fixed (held) and expansion (floating) bearing.  The proper positioning of these units is key to maximizing bearing life and equipment uptime.
Blog Thumbnail
Author: Adam Welander | Category: IIoT Smart Solutions
The Model 1030, the newest addition to the Rexnord Smart Condition Monitoring System, has two distinctive features:  
  • It monitors oil quality along with temperature and vibration—the only such system for large gear drives.  
  • It’s universal. The Model 1030 can be fitted to nearly any gear drive with an oil port 3/4” or greater—typically on equipment with a 100 HP or larger motor.
Blog Thumbnail
Author: Dale Stallard | Category: Bearings
One of the most common reasons for bearing failure in agricultural equipment is moisture ingression. This occurs because the equipment is typically used for a limited period of time each season, therefore, it can remain idle for up to nine months at a time.
Blog Thumbnail
Author: Jason Ludwig | Category: Bearings
In agriculture, the leading cause of bearing failure is improper or inadequate lubrication and contamination ingression. For applications such as tillers, planters, harvesters and other equipment where bearings are routinely subjected to (or submerged in) dirt, sand and other contaminants, proper lubrication is critical to bearing service life.
Blog Thumbnail
Author: Dennis Bozych | Category: Bearings
Agricultural equipment endures extremely dirty environments. Metallic sleeve bearings -- commonly used in pivoting (oscillating) applications – require external lubrication with grease or oil to function properly and efficiently. However, a film of oil on the shaft acts like a magnet for environmental dirt and other contaminants.
Blog Thumbnail
Author: Mark Czubak | Category: Bearings
When it comes to dirt getting into bearings, the agriculture industry tops the chart. Whether you're plowing, harvesting, tilling or discing, the bearings in these applications experience some of the worst contamination possible. We all know that when the work begins, uptime is crucial, and nothing increases cost more than a piece of farm machinery that’s been sidelined during the peak season.